Control Icon Guide - Next Generation Control - Mill

SETUP_LOCK_NGC_icon
SETUP_LOCK_NGC_icon

Setup

Setup mode is locked; the control is in Run mode. Most machine functions are disabled or limited while the machine doors are open.

SETUP_UNLOCK_NGC_icon
SETUP_UNLOCK_NGC_icon

Setup

Setup mode is unlocked; the control is in Setup mode. Most machine functions are available, but may be limited while the machine doors are open.

WARNING_DOOR_OPEN_NGC_icon
WARNING_DOOR_OPEN_NGC_icon

Door Open

WarningDoor is open.

RUNNING_NGC_icon
RUNNING_NGC_icon

Running

The machine is running a program.

POWER_SAVING_SERVOS_OFF_NGC_icon
POWER_SAVING_SERVOS_OFF_NGC_icon

Power Saving

The power-saving servos-off feature is active. Refer to Setting 216 for more information.

JOG_NGC_icon
JOG_NGC_icon

Jog

An axis is jogging at the current jog rate.

JOG_RETURN_NGC_icon
JOG_RETURN_NGC_icon

Jog

This icon appears while the control returns to the workpiece during a run-stop-jog-continue operation.

JOG_HOLD_NGC_icon
JOG_HOLD_NGC_icon

Jog

You have pressed FEED HOLD during the return portion of a run-stop-jog-continue operation.

JOG_AWAY_NGC_icon
JOG_AWAY_NGC_icon

Jog

This icon prompts you to jog away during a run-stop-jog-continue operation.

FEED_HOLD_NGC_icon
FEED_HOLD_NGC_icon

Feed Hold

The machine is in feed hold. Axis motion has stopped, but the spindle continues to turn.

FEED_NGC_icon
FEED_NGC_icon

Feed

The machine is executing a cutting move.

RAPID_NGC_icon
RAPID_NGC_icon

Rapid

The machine is executing a non-cutting axis move (G00) at the fastest possible rate. Overrides can affect the actual rate.

DWELL_NGC_icon
DWELL_NGC_icon

Dwell

The machine is executing a dwell (G04) command.

RESTART_NGC_icon
RESTART_NGC_icon

Restart

The control scans the program before a restart if Setting 36 is ON.

SINGLE_BLOCK_STOP_NGC_icon
SINGLE_BLOCK_STOP_NGC_icon

Singbk Stop

SINGLE BLOCK mode is active, and the control needs a command to continue.

DOOR_HOLD_NGC_icon
DOOR_HOLD_NGC_icon

Door Hold

Machine motion has stopped because of door rules.

JOG_LOCK_NGC_icon
JOG_LOCK_NGC_icon

Jog Lock

Jog lock is active. If you press an axis key, that axis moves at the current jog rate until you press JOG LOCK again, or the axis reaches its limit.

REMOTE_JOG_NGC_icon
REMOTE_JOG_NGC_icon

Remote Jog

The optional remote jog handle is active.

VECTOR_JOG_NGC_icon
VECTOR_JOG_NGC_icon

Vector Jog

For five-axis machines, the tool will jog along the vector defined by the rotary positions.

LOW_GEAR_BOX_OIL_FLOW_LOW_GEAR_BOX_OIL_LEVEL_NGC_icon
LOW_GEAR_BOX_OIL_FLOW_LOW_GEAR_BOX_OIL_LEVEL_NGC_icon

Gear Box Lube

The spindle gear box oil level is low.

LOW_ROTARY_OIL_FLUID_NGC_icon
LOW_ROTARY_OIL_FLUID_NGC_icon

Rotary Lube

Check and fill the rotary table lubrication oil reservoir.

TSC_ON_NGC_iconTSCFILTER
TSC_ON_NGC_iconTSCFILTER

TSC Filter Off

Clean the Through-Spindle Coolant filter.

LOW_COOLANT_CONCENTRATE_NGC_icon
LOW_COOLANT_CONCENTRATE_NGC_icon

Low Coolant

Fill the concentrate reservoir for the coolant refill system.

LOW_LUBE_NGC_icon
LOW_LUBE_NGC_icon

Low Lube

The spindle lubrication oil system detected a low oil condition, or the axis ball screw lubrication system detected a low grease or low pressure condition.

LOW_OIL_NGC_icon
LOW_OIL_NGC_icon

Low Oil

The rotary brake oil level is low.

MIST_FILTER_OFF_NGC_iconMISTFILTER
MIST_FILTER_OFF_NGC_iconMISTFILTER

Mist Filter

Mist filter is off.

WARNING_LOW_COOLANT_NGC_icon
WARNING_LOW_COOLANT_NGC_icon

Coolant Warning

Coolant level is low.

LOW_AIR_FLOW_NGC_iconCFM
LOW_AIR_FLOW_NGC_iconCFM

Low Air Flow

Inch Mode - Air flow is not sufficient for correct machine operation

LOW_AIR_FLOW_IPM_NGC_iconl/min
LOW_AIR_FLOW_IPM_NGC_iconl/min

Low Air Flow

Metric Mode - Air flow is not sufficient for correct machine operation.

MAINTENANC_DUE_NGC_icon
MAINTENANC_DUE_NGC_icon

Maintenance

A maintenance procedure is due, based on information in the MAINTENANCE page. The maintenance page is part of Current Commands.

HANDLE_SPINDLE_NGC_icon
HANDLE_SPINDLE_NGC_icon

Spindle

When you press HANDLE SPINDLE, the jog handle varies the spindle override percentage.

HANDLE_FEED_NGC_icon
HANDLE_FEED_NGC_icon

Spindle

When you press HANDLE FEED, the jog handle varies the feed rate override percentage.

HANDLE_TEXT_SCROLL_NGC_icon
HANDLE_TEXT_SCROLL_NGC_icon

Text Scroll

When you press HANDLE SCROLL, the jog handle varies the spindle override percentage.

MIRRORING_ON_NGC_icon
MIRRORING_ON_NGC_icon

Mirroring

Mirroring mode is active. Either G101 is programmed or Setting 45, 46, 47, 48, 80, or 250 (mirror image of axis X, Y, Z, A, B, or C) is set to ON.

MIRRORING_RIGHT_NGC_icon
MIRRORING_RIGHT_NGC_icon

Mirroring

Mirroring mode (G101) is active. Mirror Right.

MIRRORING_LEFT_NGC_icon
MIRRORING_LEFT_NGC_icon

Mirroring

Mirroring mode (G101) is active. Mirror Left.

BRAKE_UNCLAMPED_NGC_icon
BRAKE_UNCLAMPED_NGC_icon

Brake

A rotary axis brake, or a combination of rotary axis brakes, is unclamped.

BRAKE_CLAMPED_NGC_icon
BRAKE_CLAMPED_NGC_icon

Brake

A rotary axis brake, or a combination of rotary axis brakes, is clamped.

WARNING_LOW_VOLTAGE_NGC_icon
WARNING_LOW_VOLTAGE_NGC_icon

Low Voltage

The Power Fault Detect Module (PFDM) detects low incoming voltage. If the condition continues, the machine cannot continue operation.

ALARM_LOW_VOLTAGE_NGC_icon
ALARM_LOW_VOLTAGE_NGC_icon

Low Voltage

The Power Fault Detect Module (PDFM) detects incoming voltage that is too low to operate. The machine will not operate until the condition is corrected.

WARNING_HIGH_VOLTAGE_NGC_icon
WARNING_HIGH_VOLTAGE_NGC_icon

High Voltage

The PFDM has detected incoming voltage above a set limit, but still within operating parameters. Correct the condition to prevent damage to machine components.

ALARM_HIGH_VOLTAGE_NGC_icon
ALARM_HIGH_VOLTAGE_NGC_icon

High Voltage

The PFDM has detected incoming voltage that is too high to operate and could cause damage to the machine. The machine will not operate until the condition is corrected.

WARNING_HIGH_AIR_NGC_icon
WARNING_HIGH_AIR_NGC_icon

High Air

The air pressure to the machine is too high to reliably operate pneumatic systems. Correct this condition to prevent damage to or incorrect operation of pneumatic systems. You may need to install a regulator at the machine’s air input.

ALARM_HIGH_AIR_NGC_icon
ALARM_HIGH_AIR_NGC_icon

High Air

The air pressure to the machine is too high to operate pneumatic systems. The machine will not operate until the condition is corrected. You may need to install a regulator at the machine’s air input.

WARNING_LOW_AIR_NGC_icon
WARNING_LOW_AIR_NGC_icon

Low Air

The air pressure to the machine is too low to reliably operate pneumatic systems. Correct this condition to prevent damage to or incorrect operation of pneumatic systems.

ALARM_LOW_AIR_NGC_icon
ALARM_LOW_AIR_NGC_icon

Low Air

The air pressure to the machine is too low to operate pneumatic systems. The machine will not operate until the condition is corrected. You may need a higher-capacity air compressor.

ESTOP1_PENDANT_NGC_icon1
ESTOP1_PENDANT_NGC_icon1

E-Stop

EMERGENCY STOP on the pendant has been pressed. This icon disappears when EMERGENCY STOP is released.

ESTOP2_PALLET_CHANGER_NGC_icon2
ESTOP2_PALLET_CHANGER_NGC_icon2

E-Stop

EMERGENCY STOP on the pallet changer has been pressed. This icon disappears when EMERGENCY STOP is released.

ESTOP3_TOOL_CHANGER_NGC_icon3
ESTOP3_TOOL_CHANGER_NGC_icon3

E-Stop

EMERGENCY STOP on the tool changer cage has been pressed. This icon disappears when EMERGENCY STOP is released..

ESTOP4_AUXILIARY_DEVICE_NGC_icon4
ESTOP4_AUXILIARY_DEVICE_NGC_icon4

E-Stop

EMERGENCY STOP on an auxiliary device has been pressed. This icon disappears when EMERGENCY STOP is released.

SINGLE_BLOCK_ACTIVE_NGC_icon
SINGLE_BLOCK_ACTIVE_NGC_icon

Single Blk

SINGLE BLOCK mode is active. The control executes programs (1) block at a time. Press CYCLE START to execute the next block.

WARNING_TOOL_LIFE_NGC_icon
WARNING_TOOL_LIFE_NGC_icon

Tool Life

The tool life remaining is below Setting 240, or the tool is the last one in the tool group.

ALARM_TOOL_LIFE_NGC_icon
ALARM_TOOL_LIFE_NGC_icon

Tool Life

The tool or tool group has expired, and no replacement tools are available.

OPTIONAL_STOP_NGC_icon
OPTIONAL_STOP_NGC_icon

Opt Stop

OPTIONAL STOP is active. The control stops the program at each M01 command.

BLOCK_DELETE_NGC_icon
BLOCK_DELETE_NGC_icon

Blk Delete

BLOCK DELETE is active. The control skips program blocks that begin with a slash (/).

TOOL_CHANGER_DOOR_OPEN_NGC_icon
TOOL_CHANGER_DOOR_OPEN_NGC_icon

TC Door Open

The side-mount tool changer door is open.

TL_CCW_NGC_icon
TL_CCW_NGC_icon

TL CCW

The side-mount tool changer carousel is rotating counter-clockwise.

TL_CW_NGC_icon
TL_CW_NGC_icon

TL CW

The side-mount tool changer carousel is rotating clockwise.

TOOL_CHANGE_NGC_icon
TOOL_CHANGE_NGC_icon

Tool Change

A tool change is in progress.

TOOL_UNCLAMPED_NGC_icon
TOOL_UNCLAMPED_NGC_icon

Tool Unclamped

The tool in the spindle is unclamped.

TOOL_PROBE_NGC_icon
TOOL_PROBE_NGC_icon

Tool Probe

Indicates the tool probe is active.

CONVEYOR_FORWARD_NGC_icon
CONVEYOR_FORWARD_NGC_icon

Conveyor Forward

The conveyor is active and moving forward.

CONVEYOR_REVERSE_NGC_icon
CONVEYOR_REVERSE_NGC_icon

Conveyor Reverse

The conveyor is active and moving in reverse.

TSC_NGC_icon
TSC_NGC_icon

TSC

The Through-Spindle Coolant (TSC) system is active.

TAB_NGC_icon
TAB_NGC_icon

TAB

The Tool Air Blast (TAB) system is active.

AUTO_AIR_GUN_NGC_icon
AUTO_AIR_GUN_NGC_icon

Air Blast

The Auto Air Gun is active.

HIL_NGC_icon
HIL_NGC_icon

HIL

Indicates the optional High Intensity Lights (HIL) are turned ON and the doors are open. Duration is determined by Setting 238.

COOLANT_REFILL_NGC_icon
COOLANT_REFILL_NGC_icon

Coolant Refill

Coolant Refill feature is actively mixing and adding coolant to the tank.

COOLANT_ON_NGC_icon
COOLANT_ON_NGC_icon

Coolant On

The main coolant system is active.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.