Wired Probe System - Troubleshooting Guide

  1. OMP40 work probe: A spindle-mounted wireless probe that communicates with an optical interface.
  2. Work probe stylus: The part of the work probe that touches parts during measurement.
  3. Tool probe stylus: The part of the tool probe that tools touch during measurement. Tools touch the top and side of the stylus when the probe measures tool length and diameter.
  4. TS27R tool probe: The table-mounted TS27R has no batteries or optical interface. This is a wired probe.
  5. Tool probe cable: This cable carries signals from the tool probe to the CNC control.
  6. OMI Optical Machine Interface: The wireless interface for the OMP40 work probe. The OMI uses infrared light to communicate with the CNC control and switch the probe on or off.
  7. OMI cable: This cable connects the OMI to the CNC control.

Work probes for Wireless Probe System (WIPS) do not work in the wired probe systems (VQCPS).

  • The VCQPS work probe (P/N 60-0024) has a square Haas logo.
  • The WIPS work probe (P/N 60-0050) has a round Haas logo.
Work Probe Operation Tool Probe Operation

To power on the work probe, enter this program in MDI:

M53;
G04 P2.;
Push CYCLE START.

The LEDs on the work probe flash green when the probe is powered on and ready for use. When the probe stylus is touched, a “beep” sound is made by the CNC control. The LEDs on the work probe flash red each time the stylus is touched.

To power off the work probe, enter this code in MDI:

M63;

To power on the wired tool probe, enter this program in MDI:

M52;
Push CYCLE START.

When the stylus on the tool probe is touched, the CNC control makes a "beep" sound.

The tool probe does not have any LEDs.

To power off the wired tool probe, enter this program in MDI:

M62;

OMI Operation

[1] CNC control is powered on. The probe is not in use.

[2] M53 commanded. The OMI is sending a start signal to the work probe to power it on or power it off.

[3] The work probe is powered on and ready for use.

[4] The stylus has been touched. The OMI is sending a skip signal to the CNC control.

Symptom Possible Cause Corrective Action
Alarm 1101 PROBE STARTUP FAILURE. Bad batteries. Replace the batteries.
The macros are corrupted. Reload the macros
Settings in the work probe are not correct. Correct the settings.
Alarm 1092 PROBE OPEN. Alarm 1093 PROBE FAIL. Interference from the work lights. Adjust the work lights.
Settings in the work probe are not correct. Correct the settings.
The surface of the part was not found. Edit the program.
The tool probe does not beep/activate. The macros are corrupted. Reload the macros
The OMI LEDs do not turn green. The macros are corrupted. Reload the macros
Incorrect measurements. The probe is not calibrated. Calibrate the probe.

Macros

Corrective Action:

The wired probe system uses Renishaw VQCPS macro version 1.9. Download the file that has these macros from diy.haascnc.com.

Click on the search tab in the upper right corner. Type Probing.

Select Renishaw – Probe Macro – Haas VQC – Wired Table Probe, English Inch/MM, V1.9

After you load this program file into the CNC control, make sure Setting 26, 9xxx PROGS EDIT LOCK, is set to 1. This prevents all of the Macro programs from being edited or deleted.

Surface Not Found

Corrective Action:

Refer to Wireless Intuitive Probe System - WIPS - Troubleshooting Guide

Settings

Corrective Action:

A procedure to verify the probe settings is included in the Renishaw Probes Installation guide. Go to Mill - Renishaw Probes - Installation on diy.haascnc.com.

note: Do not touch the stylus when you install the batteries. This can change the settings.

To change the probe settings you move the stylus in a specified order. Refer to the illustration to see the specified order.

The Illustration shows these symbols: The symbols tells you this: This gives this result:
A red arrow that points to the right. Move and hold the stylus for less than (4) seconds. Selects the next option within a group.
A green arrow that points down. Move and hold the stylus for more than (4) seconds. Moves from one group to another.
A white arrow that points down. Do not touch the stylus for (20) seconds or more. Exits the set up.

Calibration

Corrective Action:

The probes need to be calibrated anytime a stylus has been replaced, the table probe has been moved, or if the CNC control generates alarms during probe routines. Follow the procedure for calibrating the Table Probe and the Spindle Probe. Go to Mill - Probing with VQC Templates on diy.haascnc.com for probing with VQC templates.

This procedure includes instructions for calibrating the probes. The probes must be calibrated in this order:

  1. Table Probe
  2. Spindle Probe Length
  3. Spindle Probe Diameter

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback