Renishaw - WIPS - Optical Machine Interface (OMI) - Lights Information

Number in the Illustration LED Name LED Color This tells you this information:
1 Probe 1 Green Probe 1 is active. Usually the spindle probe is probe 1.
2 Start signal status The LED flashes yellow (1) time. A machine start signal is commanded.
The LED flashes yellow many times. The system is set to Auto Start mode.
3 Low Bat Red The battery is low.
4 Probe Status

Green

The probe is seated.

Red

The probe is triggered or an error has occurred.

5 Probe 2 Green Probe 2 is active. Usually the table probe is probe 2.
6 Signal Strength

Green

The signal is good.

Yellow

The signal is weak or blocked.

Red

The probe does not receive the signal.

7 Error

Red

The probe is not transmitting.

Blue

Refer to the user's guide.

Yellow

Refer to the user's guide.

Purple

Refer to the user's guide.

Be aware: Many service and repair procedures should be done only by authorized personnel. The service technicians at your Haas Factory Outlet (HFO) have the training, experience, and are certified to do these tasks safely and correctly. You should not do machine repair or service procedures unless you are qualified and knowledgeable about the processes.

Danger: Some service procedures can be dangerous or life-threatening. DO NOT attempt a procedure that you do not completely understand. Contact your Haas Factory Outlet (HFO) and schedule a service technician visit if you have any doubts about doing a procedure.

Feedback